ALWAYS DOWNLOAD THE LATEST VERSION OF REVIT CONTENT BEFORE USING THEM IN A NEW PROJECT.

This change history file can be used to help you determine whether or not the changes
in the latest version available warrant the effort to update a family that is already
being used in an existing project.


Family File Dates: 2013 October 1
  - Rebranded to Daikin Applied


Family File Dates: 2011 March 29
  - "Include Clearance" yes/no (checkbox) instance parameter now controls clearance volume     existence (replaces "Clearance Type" parameter)
  - Added "Parts Catalog URL" parameter, for long-term facilities managers to quickly access     replacement parts info.
  - Assembly Code values are now compliant with MasterFormat 2010 (can be helpful for e-SPECS     users)
  - Simplified the type catalogs


Family File Dates:  xxxxxxxx
  - Added data to 'ParameterName' to make columns unique where required



Family File Dates:  2010 June 28
  - Added families for the AZ self-contained units
  - Changed Ventilation Air duct connectors from a System Type of Supply Air to Return Air
    - Makes it easier to connect to Autodesk's external louver families
  - Changed AV clearances to only encompass the main box (not extend out with draftstops)
  - Corrected the product documentation link on some families



Family File Dates: 2010 May 28
  - Initial Release